With over a trillion IoT devices expected to connect to the cloud in the coming years, the challenge is that there is not enough bandwidth to process all the information within central data centers. To alleviate this pipeline limitation, there will be an increasing focus on data processing at the edge of the network to provide useful and actionable insights at the local application level. An example of this problem is intelligent security, which provides monitoring and surveillance either through audio or video processing.

Key Features

  • High performance and suitable MPU RZ/A2M with embedded 4MB RAM, Dynamically Reconfigurable Processor (DRP) technology
  • Rich connection interface, including MIPI for camera, 2Port Ethernet, RS-485, USB, CAN, Hyper-Bus
  • Full Renesas RS-485 transceiver, DC/DC, LDO, temperature/humidity sensor device portfolio

Block Diagram

Recommended Products

ProductDescriptionDatasheetOrdering
RZ/A2MHigh-speed embedded AI-based image processing device with dynamically reconfigurable processor (DRP) technology Buy Now
ISL80505High performance 500mA LDOBuy Now
ISL80020Compact synchronous buck converter Buy Now
HS3002High performance relative humidity and temperature sensor Buy Now
ISL814875V, half duplex, 5Mbps, RS-485/RS-422 transceiverBuy Now